Use this panel to specify the command, options, and expert settings for DSC Disassembler.
The following table lists and describes the disassembler options for DSC.
| Option | Description |
|---|---|
| Command | Shows the location of the preprocessor executable file. Default value is ""${DSC_ToolsDir}/mwld56800e". You can specify additional command line options for the preprocessor; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the linker will be called with. |
| Expert settings | |
| Command line pattern | Shows the command line pattern; default is ${COMMAND} -dis ${FLAGS} ${INPUTS} |