Use this panel to specify the command, options, and expert settings for the build tool assembler. Additionally, the Assembler tree control includes the general and include file search path settings.
The following table lists and describes the compiler optimization options for DSC.
| Option | Description |
|---|---|
| Command | Shows the location of the assembler executable file. You can specify additional command line options for the assembler; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the assembler will be called with. |
| Expert Settings | |
| Command line pattern | Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${OUTPUT_FLAG} ${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}. |