ColdFire Preprocessor

Use this panel to specify preprocessor behavior and define macros.

The following table lists and describes the preprocessor options for ColdFire.

Table 1. Tool Settings - ColdFire Preprocessor Options
Option Description
Command Shows the location of the preprocessor executable file. You can specify additional command line options for the preprocessor; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the preprocessor will be called with
Expert Settings Shows the command line pattern; default ${COMMAND} ${FLAGS} ${INPUTS}
Command line pattern