Use this panel to specify the command, options, and expert settings for ColdFire Disassembler.
The following table lists and describes the ColdFire disassembler options.
| Option | Description |
|---|---|
| Command | Shows the location of the linker executable file. You can specify additional command line options for the linker; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the linker will be called with |
| Expert Settings | Shows the command line pattern; default is ${COMMAND} -dis ${FLAGS} ${INPUTS} |
| Command line pattern |