ColdFire Assembler

Use this panel to specify the command, options, and expert settings for the build tool assembler. Additionally, the Assembler tree control includes the general and include file search path settings.

The following table lists and defines each option of the ColdFire Assembler panel.

Table 1. Tool Settings - ColdFire Assembler Options
Option Description
Command Shows the location of the assembler executable file. You can specify additional command line options for the assembler; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the assembler will be called with.
Expert Settings Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${OUTPUT_FLAG} ${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}.
Command line pattern