Burner

Use the Burner for ColdFire Preference Panel to map *.bbl (batch burner language) files to the Burner Plug-In. When the project folder contains a *.bbl file, *.bbl file processing during the post-link phase uses the settings in the Burner preference panel.

The following table lists and describes the burner options for ColdFire.

Table 1. Tool Settings - Burner Options
Option Description
Command Shows the location of the burner executable file. Default value is: "${HC08Tools}/burner.exe". You can specify additional command line options for the burner; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the burner will be called with.
Expert Settings  
Command line pattern Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${INPUTS}.