Build Properties for RS08

The Properties for <project> window shows the corresponding build properties for an RS08 project.

Figure 1. Build Properties - RS08
Build Properties - RS08

The following table lists the build properties specific to developing software for HCS08.

The properties that you specify in these panels apply to the selected build tool on the Tool Settings page of the Properties for <project> window.

Table 1. Build Properties for RS08
Build Tool Build Properties Panels
General General
S08 Disassembler S08 Disassembler > Output
  S08 Disassembler > Input
  S08 Disassembler > Host
  S08 Disassembler > Messages
  S08 Disassembler > Messages > Disable user messages
S08 Linker S08 Linker > Optimization
  S08 Linker > Output
  S08 Linker > Input
  S08 Linker > Host
  S08 Linker > Messages
  S08 Linker > Messages > Disable user messages
  S08 Linker > General
S08 Burner S08 Burner > Output > Configure S-Record
  S08 Burner > Input
  S08 Burner > Host
  S08 Burner > Messages
  S08 Linker > Messages > Disable user messages
  S08 Burner > General
RS08 Compiler RS08 Compiler > Output
  RS08 Compiler > Output > Configure Listing File
  RS08 Compiler > Output > Configuration for list of included files in make format
  RS08 Compiler > Input
  RS08 Compiler > Language
  RS08 Compiler > Language > CompactC++ features
  RS08 Compiler > Host
  RS08 Compiler > Code Generation
  RS08 Compiler > Messages
  RS08 Compiler > Messages > Disable user messages
  RS08 Compiler > Preprocessor
  RS08 Compiler > Type Sizes
  RS08 Compiler > General
  RS08 Compiler > Optimization
  RS08 Compiler > Optimization > Mid level optimizations
  RS08 Compiler > Optimization > Mid level branch optimizations
  RS08 Compiler > Optimization > Tree optimizer
  RS08 Compiler > Optimization > Optimize Library Function
RS08 Assembler RS08 Assembler > Output
  RS08 Assembler > Output > Configure Listing File
  RS08 Assembler > Input
  RS08 Assembler > Language
  RS08 Assembler > Language > Compatibility modes
  RS08 Assembler > Host
  RS08 Assembler > Code Generation
  RS08 Assembler > Messages
  RS08 Assembler > Messages > Disable user messages
  RS08 Assembler > General
RS08 Preprocessor RS08 Preprocessor > Preprocessor Settings