ARM Linker > General

Use this panel to specify the general linker behavior.

The following table lists and describes the general linker options for ARM.

Table 1. Tool Settings - ARM Linker > General Options
Option Description
Other Flags Specify additional command line options for the linker; type in custom flags that are not otherwise available in the UI.