Use this panel to control how the disassembler formats the listing file, as well as error and warning messages. You can specify verbosity of messages, whether to show headers, core modules, extended mnemonics, addresses, object or source code, ldata modules, exception tables, and debug information.
The following table lists and describes the ARM disassembler settings.
| Option | Description |
|---|---|
| Show Headers | Check to display headers in the listing file; disassembler writes listing headers, titles, and subtitles to the listing file. |
| Show Symbol and String Tables | Check to display symbol and string tables directives to the listing file. |
| Verbose Info | Check to shows each command line that it passes to the shell, along with all progress, error, warning, and informational messages that the tools emit. |
| Show Relocations | Check to have the disassembler show information about relocated symbols. Clear to prevent the disassembler from showing information about relocated symbols. |
| Show Code Modules | Check to show code modules in the listing file. |
| Show Extended Mnemonics | Check to show the extended mnemonics in the listing file. |
| Show Addresses and Opcodes | Check to show the addresses and object code in the listing file. |
| Show Source Code | Check to show the source code in the listing file. |
| Show Comments | Check to show the comments in the listing file. |
| Show Data Modules | Check to show the data modules in the listing file. |
| Disassemble Exception Tables | Check to disassemble exception tables in the listing file. |
| Show Debug Info | Check to generate symbolic information for debugging the build target. |