ARM Assembler > General

Use this panel to specify the general assembler behavior.

The following table lists and describes the general assembler options for ARM.

Table 1. Tool Settings - ARM Assembler > General Options
Option Description
Label Must End With `:' Clear if system does not require labels to end with colons. By default, the option is checked.
Directives Begin With `.' Clear if the system does not require directives to start with periods. By default, the option is checked.
Allow Space In Operand Field Clear to restrict the assembler from adding spaces in operand fields. By default, the option is checked.
Case-Sensitive Identifier Clear to instruct the assembler to ignore case in identifiers. By default, the option is checked.
Enable GNU Assembler Compatible Syntax Instructs the assembler to accept GNU-style assembly syntax.
Enable ARM ADS Compatible Syntax Instructs the assembler to accept ARM ADS compatible syntax extensions.
Other Flags Specify additional command line options for the assembler; type in custom flags that are not otherwise available in the UI.