The settings in the launch configurations handles all core-specific initializations. To set up the launch configurations, perform these steps.
- Ensure that you machine has USB NEXUS Multilink connected to a Leopard (MPC5643L) DPM board.
- Select Run > Debug Configurations.
A menu of launch configurations appears.
Figure 1. Debug Configurations Dialog Box
- Select the core or cores to be debugged using the Target checkboxes. In this case you can debug core 0 or both cores.
- Click Debug.
- Debugger halts execution at first statement of main().
The Debug view displays all the threads associated with the core.
Figure 2. Multicore Debugging - Debug Core 0 
- Repeat steps one through four to download all the other cores.
Figure 3. Multicore Debugging - Debug All Cores 
Note: When you enter debug, the DPM project will show you two cores, first stopped at main() and the second stopped at __start_p1. For the LSM project you will see only one core stopped at main().
- Select a thread from core 0 in the Debug view.
All the views in the
Debug
perspective will be updated to display the debug session for
the selected core.
Figure 4. Debugging a LSM Project 
Figure 5. Viewing Debug Information for Core 0