- Select the desired connection from the Connection to be used group. For example, check the P&E Full Chip Simulation checkbox.
Note: You can select multiple connections by checking appropriate checkboxes in the Connections page.
- Click Finish .
The
Import MCU Executable
window closes and the wizard creates a project
according to your specifications. You can access the project from the
CodeWarrior Projects view
in the
Workbench
window.
Figure 1. CodeWarrior Projects View 
- Right-click on the project and from the context menu select Build Project .
The new project is ready for use. You can now customize it by adding your own source
code files, changing debugger settings, or adding libraries.