Remote

When debugging a Linux application, use this tab to specify where the debugger downloads the program for debug on the Linux host system, and whether to launch any optional applications while debugging.

The following figure shows the Remote tab view.

Figure 1. Remote Tab
Remote Tab

The following table describes the Remote tab settings.

Table 1. Remote Tab Settings
Option Description
Remote download path Specifies the directory path that the debugger downloads the test program into.
Launch remote host application Specifies the directory path of a Linux program that is to be launched along with the test program.