Import a MCU Executable File Page

Use this page to name your new project, and specify the workspace directory.

Figure 1. Import MCU Executable - Import a MCU Executable File Page
Import MCU Executable - Import a MCU Executable File Page

The following table describes the purpose of the various options.

Table 1. Import a MCU Executable File Page Settings
Option Description
New Project Name Enter the name for the new project in this text box.
Use default location Stores the files required to build the program in the Workbench's current workspace directory. The project files are stored in the default location. Uncheck the Use default location checkbox and click Browse to specify a new location.
Location Specifies the directory that contains the project files. Click Browse to navigate to the desired directory. This option is only available when Use default location checkbox is clear.
Choose file system Specifies the file system to use. However, this option is available only when Use default location checkbox is clear. You can select either the default file system or a Target Management via Remote System Explorer (RSE).