Adding Memory Rendering

You can use the Renderings pane of the Memory view to examine the memory content, starting at any valid address. The information displayed in this page is read only and cannot be used to modify the memory content.

To add a new memory rendering, perform these steps.

  1. Start a debugging session.
  2. Open the Memory view.
  3. In the Monitors pane, select the memory monitor for which you want to add a memory rendering.
    Note: To create a memory monitor, right-click a blank area in the Monitors pane and select Add Memory Monitor. Alternatively, click the plus-sign
    icon in the Monitors pane toolbar.
  4. Click the New Renderings tab to select renderings.
    Figure 1. New Renderings View
    New Renderings View
  5. Select a rendering type from the Select rendering(s) to create list and click the Add Rendering(s) button. Alternatively, right-click in the Renderings pane and select Add Rendering from the context menu. For example, select Disassembly.
  6. Click Rendering(s) .

    The selected memory rendering type appears in the Memory view.

    Figure 2. Added Rendering
    Added Rendering