S12Z derivatives

If you select an S12Z board or derivative in the Devices page, the Connections page appears.

Figure 1. Connections Page - S12Z Derivative
Connections Page - S12Z Derivative

The table below explains the connections available on the Connections page.

Table 1. Connections Page Settings for S12Z Derivative
Option Description
P&E USB MultiLink Universal [FX] / USB MultiLink Connects to the P&E USB MultiLink Universal [FX] / USB MultiLink.
P&E Cyclone Connects to the P&E Cyclone(USB default).
P&E TraceLink Connect to P&E TraceLink (USB default).
Open Source BDM Connects to the Open Source BDM.