Qorivva derivatives

If you select a Qorivva board or derivative in the Devices page, the Connections page appears.

Figure 1. Connections Page - Qorivva Derivatives
Connections Page - Qorivva Derivatives

The table below explains the connections available on the Connections page.

Table 1. Connections Page Settings for Qorivva Derivatives
Option Description
P&E USB MultiLink PPCNEXUS Connects to the P&E USB MultiLink PPCNEXUS.
P&E USB MultiLink Universal [FX] / USB MultiLink Connects to the P&E USB MultiLink Universal [FX] / USB MultiLink.
P&E Cyclone Connects to the P&E Cyclone (USB default).
Open Source JTAG Connects to the Open Source JTAG.
Note: The CodeWarrior debugger supports NEXUS ISTO IEEE 5001-2003 and NEXUS ISTO IEEE 5001-2010 for Qorivva families.