The Microcontrollers New Bareboard Project wizard presents a series of pages that prompt you for the features and settings to be used when making your program. For example, the devices options lets you select the derivative or board you would like to use. This wizard also helps you specify other settings, such as whether the program executes on an emulator or simulator rather than actual hardware, and the characteristics of the connection that communicates with a hardware target.
This topic describes the various pages that the wizard displays as it assists you in creating a bareboard project. The pages of the wizard can differ based on the project type or execution target.
The pages of the New Bareboard Project wizard are: