To create a new target board project for a ColdFire V2/V3/V4/V4e/Vx derivative using the
New Bareboard Project
wizard:
- Launch the Workbench.
- Select File > New > Bareboard Project , from the IDE menu bar.
The
Create an MCU bareboard Project
page of the New Bareboard Project
wizard
appears.
- Specify a name for the new project. For example, enter the project name as TargetProject_2.
Note: If you do not want to use the default location, clear the Use default location checkbox. In the Location text box, enter the full path of the directory in which you want to create your project including the project name. Alternatively, click Browse and select the desired location from the Browse For Folder dialog box and click OK. Ensure that you append the path with the name of the project to create a new location for your project.
Figure 1. New Bareboard Project Wizard - Create an MCU Bareboard Project Page 
- Click Next.
The Devices page appears.
- Expand the desired tree control and select the derivative or board you would like to use. For example, select ColdFire V4e > MCF547X > MCF5475.
Figure 2. New Bareboard Project Wizard - Devices Page
- Click Next.
The Connections page appears.
Figure 3. New Bareboard Project Wizard - Connections Page 
- Check the appropriate connection.
Note: You can select multiple connections by checking appropriate checkboxes in the Connections page. By default, the P&E USB MultiLink Universal [FX] / USB MultiLink checkbox is checked.
- Click Next.
The ColdFire Build Options
page appears.
Figure 4. New Bareboard Project Wizard - ColdFire Build Options Page 
- Select the appropriate options to enable C++ support, hardware startup level, and the optimization level for your project.
- Click Finish.
The wizard creates a new target board project for the ColdFire V4e architecture. You
can access the project from the
CodeWarrior Projects
view in the Workbench
window.
Figure 5. CodeWarrior Projects View 
The new project is ready for use. You can now customize it by adding your own source code files, changing debugger settings, or adding libraries.
Note: You can click Finish at any step in the Project Wizard to save the project with the default settings.