Use this page to specify the project name and the directory where the project files are located.
The table below describes the purpose of the various options.
| Option | Description |
|---|---|
| Project Name | Enter the name for the new project in this text box. Note: Do not use the reserved/special characters/symbols such as < (less than), > (greater than), : (colon), " (double quote), / (forward slash), \ (backslash), | (vertical bar or pipe), ? (question mark), @ (at), * (asterisk) in the project name. sing special characters/symbols in the project name may result in an unexpected behavior. |
| Use default location | Stores the files required to build the program in the Workbench's current workspace directory. The project files are stored in the default location. Clear the Use default location checkbox and click Browse to select a new location. |
| Location | Specifies the directory that contains the project files. Click Browse to navigate to the desired directory. This option is available only when Use default location checkbox is clear. |