Create a Linux/uClinux Application Project Page

Use this page to specify the project name and the directory where the project files are located.

Figure 1. Create a Linux/uClinux Application Project page
Create a Linux/uClinux Application Project Page

The table below describes the purpose of the various options.

Table 1. Create a Linux/uClinux Application Project Page Settings
Option Description
Project Name Enter the name for the new project in this text box.
Use default location Stores the files required to build the program in the Workbench's current workspace directory. The project files are stored in the default location. Clear the Use default location checkbox and click Browse to select a new location.
Location Specifies the directory that contains the project files. Click Browse to navigate to the desired directory. This option is only available when Use default location checkbox is clear.