Code Size

The following table lists the library and the code size in bytes.

Table 1. Library and Code Size
Library Code Size (bytes)
ansif 1600
ansifc 2200
ansid 2500
ansidc 3200

The following table list the operation and compliance.

Table 2. Operation and Complaince
Operation Default Compliant
Float addition 300 430
Float multiplication 450 590
Float division 370 530
Float to long conversion 170 230
Double addition 360 550
Double multiplication 650 800
Double division 550 730
Double to long long conversion 280 300