To add an unprotect action to the target task, perform these steps.
- Select the Protect/Unprotect action from the Add Action drop-down list.
The Add Protect/Unprotect Action dialog box appears.
- Check the All Device check box to add an unprotect action on the full device.
- Click the Add Unprotect Action button.
- Click Done.
The Add Protect/Unprotect Action dialog box closes and the added protect or
unprotect actions appear in the Flash Programmer Actions table in the Flash
Programmer Task editor window.
Note: None of the target task restores the shadow flash user registers. If the device has some user defined configuration in shadow flash then executing the changed target task will erase the configuration also.