Reset the board. For more information, refer Hardware Reset. This step is mandatory in order to use the new LS configuration. Note: When changing the device back to DPM the shadow flash will be programmed. However, it is possible that the shadow flash sector is protected. In case the shadow flash sector is protected then the target task will fail and you will need to add an unprotect action to target task. This action need to be run before any other actions.