P&E TraceLink Ethernet

The P&E TraceLink Ethernet Connection setting permits a connection to TraceLink Ethernet devices. P&E TraceLink Ethernet mode lets you debug code, as the firmware is fully resident in the Flash of the microprocessor. The operation of all modules fully reflects the actual operation of the onboard resources. P&E’s TraceLink can conveniently support all Freescale architectures found in the current CodeWarrior 10 version; however, it can only capture the external trace signals for the ColdFire V2/3/4 and Kinetis ARM architectures
Note: S12Z devices can be debugged by the Tracelink, however Trace and Profile iscurrently not supported.
.