To change P&E's hardware interface connection settings within Debug Configurations:
- In the left column select the project for which you would like to change the settings. Within the Main tab, use the Connection selection drop-down box to select a connection.
- Then click on the Edit button beside your selected connection. The Launch Configuration Dialog will appear.
- Set the connection type to P&E DSC V234 Multilink/Multilink Universal/Cyclone MOSJTAG so that the Connection tab will populate P&E's hardware interface connection settings, as shown in the following figure.
Figure 1. P&E's Launch Configuration Dialog Box 
To use Open Source JTAG, first connect your hardware interface to your computer, and
then set the interface to USB Multilink, USB Multilink FX, Embedded OSBDM/
OSJTAG – USB Port. The Port selection should automatically populate your hardware
interface. If not, use the Refresh button and the Port selection drop-down box. If you are
having issues getting your device to populate, use the link for FAQ #29 to find popular
solutions.