Debug configurations

To change P&E's hardware interface connection settings within Debug Configurations:

  1. In the left column select the project for which you would like to change the settings. Within the Main tab, use the Connection selection drop-down box to select a connection.
  2. Then click on the Edit button beside your selected connection. The Launch Configuration Dialog will appear.
  3. Set the connection type to P&E DSC Multilink/Multilink Universal/Cyclone Pro/OSBDM so that the Connection tab will populate P&E's hardware interface connection settings, as shown in the following figure.
    Figure 1. P&E's Launch Configuration Dialog Box
    P&E's Launch Configuration Dialog Box

To use P&E’s Cyclone Ethernet, first connect your hardware interface to your computer, and then set the interface to Cyclone – Ethernet Port. The Port selection should automatically populate your hardware interface. If not, use the Refresh button and the Port selection drop-down box. You can also specify IP and Network Card IP by clicking on the checkboxes. If you are having issues getting your device to populate, use the link for FAQ #29 to find popular solutions.

Note: The Cyclone MAX does not support the ability to provide power to the target.