The P&E TraceLink allows the user to capture real-time external trace information
without having to stop or disturb the running application. This allows the user to see the
real-time execution of their code by continuously recording the processor events. For
external trace captures, the P&E TraceLink must have PST_CLK and DDATA[3:0] pin
connections from the ColdFire chip. Chips without these pins connected can still be
debugged by the TraceLink within CodeWarrior. The user must do the following to set up
external trace captures using the TraceLink.
- Right-click on the project and right-click -> Debug as -> Debug Configurations. The Debug Configuration dialog box will appear.
- In the left column, select the project type for which you would like to set the TraceLink settings.
- In the right column, select the Trace and Profile tab..
Figure 1. Trace and Profile Tab 
- Click on the Enable Trace and Profile checkbox.
- Change the other user settings that fits the users needs.
- Click on the Main tab and select the correct connection setting from the drop-down box or create a new connection by clicking on the New button.
- Once the correct connection setting is selected, click on the Edit button. The launch configuration dialog box will appear.
- When the TraceLink is selected as the interface, the Additional Options will be available. Change the Trace Max Buffer Size as the user sees fit by using the drop-down box.
Figure 2. Debugger Settings