To change P&E's hardware interface connection settings within Debug Configurations:
To use P&E's TraceLink Ethernet, first connect your hardware interface to your computer, and then set the interface to TraceLink - Ethernet Port. The Port selection should automatically populate your hardware interface. If not, use the Refresh button and the Port selection drop-down box. You can also specify IP and Network Card IP by clicking on the checkboxes. If you are having issues getting your device to populate, use the link for FAQ #29 to find popular solutions.