Once you create a project for a specific ColdFire V2/3/4 microprocessor, the debugger specifies a default algorithm to use during all Flash programming operations. The debugger uses this algorithm for nearly all programming requirements. The default algorithm can be found in the <CW_Install>/MCU/bin/plugins/support/ColdFire/gdi/P&E directory
However, you can override the default algorithm via the Alternative Algorithm function, located in the Advanced Programming/Debug Options menu. This feature can be used to select a custom programming algorithm, or select another one of P&E's many programming algorithms for use with a specific project.
Therefore it is recommended to use the default algorithm unless there is a compelling reason to do otherwise.
Use these steps to override the default algorithm:
At this point, the current project performs all future Flash programming operations using the alternative algorithm. You may revert to the default algorithm at any time by clearing the Use Alternative Algorithm checkbox.