Debug configurations

To change P&E's hardware interface connection settings within Debug Configurations:

  1. In the left column select the project for which you would like to change the settings. Within the Main tab, use the Connection selection drop-down box to select a connection.
  2. Then click on the Edit button beside your selected connection. The Launch Configuration Dialog will appear.
  3. Set the connection type to P&E RS08 Multilink/Multilink Universal/Cyclone Pro/OSBDM so that the Connection tab will populate P&E's hardware interface connection settings, as shown in the following figure.
    Figure 1. P&E's Launch Configuration Dialog Box
    P&E's Launch Configuration Dialog Box

To use P&E’s Cyclone USB, first connect your hardware interface to your computer, and then set the interface to Cyclone – USB Port. The Port selection should automatically populate your hardware interface. If not, use the Refresh button and the Port selection drop-down box. If you are having issues getting your device to populate, use the link for FAQ #29 to find popular solutions.