To change P&E's hardware interface connection settings within Debug Configurations:
- In the left column select the project for which you would like to change the settings. Within the Main tab, use the Connection Selection drop-down box to select a connection.
- Then click on the Edit button beside your selected connection. The Launch Configuration Dialog will appear.
- Set the connection type to P&E HCS08 Multilink/Multilink Universal/Cyclone Pro/OSBDM so that the Connection tab will populate P&E's hardware interface connection settings.
Figure 1. P&E's Launch Configuration Dialog Box 
To use P&E’s Cyclone USB, first connect your hardware interface to your computer, and
then set the interface to Cyclone – USB Port. The Port selection should automatically
populate your hardware interface. If not, use the Refresh button and the Port selection
drop-down box. If you are having issues getting your device to populate, use the link for
FAQ #29 to find popular solutions.