Use this panel to specify the parameter file path, startup function, object file search paths, and any additional libraries that the C/C++ Linker should use. You can specify multiple additional libraries and library search paths. Also, you can change the order in which the IDE uses or searches the libraries.
The IDE first looks for an include file in the current directory, or the directory that you specify in the INCLUDE directive. If the IDE does not find the file, it continues searching the paths shown in this panel. The IDE keeps searching paths until it finds the #include file or finishes searching the last path at the bottom of the Include File Search Paths list. The IDE appends to each path the string that you specify in the INCLUDE directive.
For example, if you see the message Could not open source file myfile.h, you must add the path for myfile.h to this panel.
The following table lists and describes the linker input options for HCS08.
| Option | Description |
|---|---|
| Parameter File | Shows the path of the parameter file. Default value is $ {ProjDirPath}/Project_Settings/Linker_Files/Project.prm. |
| Specify startup function (-E) | Defines the application entry point. |
| Search paths (-L) | Shows the list of all search paths; the ELF part of the linker searches object files first in all paths and then the usual environment variables are considered. |
| Libraries | Lists paths to additional libraries that the C/C++ linker uses. Default value is "${MCUToolsBaseDir}/lib/hc08c/lib/ansiis.lib" |
| Link case insensitive | With this option, the linker ignores object name capitalization. This option supports case-insensitive linking of assembly modules. Since all identifiers are linked case insensitive, this also affects C or C++ modules. This option only affects the comparison of names of linked objects. Section names or the parsing of the link parameter file are unaffected. They remain case sensitive. |
| Object File Format | Defines the object file format. |
The following table lists and describes the toolbar buttons that help work with the libraries and the additional object file search paths.
| Button | Description |
|---|---|
| Add - Click to open the Add directory path dialog box and specify the object file search path. | |
| Delete - Click to delete the selected object file search path. To confirm deletion, click Yes in the Confirm Delete dialog box. | |
| Edit - Click to open the Edit directory path dialog box and update the selected object file search path. | |
| Move up - Click to move the selected object file search path one position higher in the list. | |
| Move down - Click to move the selected object file search path one position lower in the list. |
The following figure shows the Add directory path dialog box.
The following figure shows the Edit directory path dialog box.
The buttons in the Add directory path and Edit directory path dialog boxes help work with the object file search paths.
The following table lists and describes the toolbar buttons that help work with the libraries and the additional object files.
| Button | Description |
|---|---|
| Add - Click to open the Add file path dialog box and specify location of the library you want to add. | |
| Delete - Click to delete the selected library path. To confirm deletion, click Yes in the Confirm Delete dialog box. | |
| Edit - Click to open the Edit file path dialog box and update the selected path. | |
| Move up - Click to move the selected path one position higher in the list. | |
| Move down - Click to move the selected path one position lower in the list. |
The following figure shows the Add file path dialog box.
The following figure shows the Edit file path dialog box.
The buttons in the Add file path and Edit file path dialog boxes help work with the file paths.