Use this panel to specify the general linker behavior.
The following table lists and describes the general linker options for HCS08.
| Option | Description |
|---|---|
| Other flags | Specify additional command line options for the linker; type in custom flags that are not otherwise available in the UI. Default value is: -WmsgSd1100 -WmsgSd1912 |