Use this panel to specify the command, options, and expert settings for the build tool linker. Additionally, the Linker tree control includes the general, libraries, and search path settings.
The following table lists and describes the linker options for HCS08.
| Option | Description |
|---|---|
| Command | Shows the location of the linker executable file. Default value is "${HC08Tools}/linker.exe". You can specify additional command line options for the linker; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the linker will be called with. |
| Expert Settings | |
| Command line pattern | Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} -add( ${INPUTS} ) |