S08 Disassembler

Use this panel to specify the command, options, and expert settings for RS08 Disassembler.

The following table lists and describes the Disassembler options.

Table 1. Tool Settings - Disassembler Options
Option Description
Command Shows the location of the disassembler executable file; default is ${HC08Tools}/decoder. You can specify additional command line options for the disassembler; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the disassembler will be called with.
Expert Settings  
Command line pattern Shows the command line patterns; default is ${COMMAND} ${FLAGS} -O${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}