Use this panel to control how the disassembler generates the input file.
The following table lists and describes the input options for RS08 disassembler.
| Option | Description |
|---|---|
| Object File Format | Defines the format of the input object files. |
| Set processor | Specifies which processor of the input object file generated for. For object files, libraries and applications, the processor is usually detected automatically. For S-Record and Intel Hex files, however, the decoder cannot determine which CPU the code is for, and therefore the processor must be specified with this option to get a disassembly output. Without this option, only the structure of a S-Record file is decoded. The following values are supported: HC08, HC08:HCS08, HC11, HC12, HC12:CPU12, HC12:HCS12, HC12:HCS12X, HC16, M68k, MCORE, PPC, RS08, 8500, 8300, 8051 and XA. |