Use this panel to specify the command, options, and expert settings for S08 Disassembler.
The following table lists and describes the Disassembler options.
| Option | Description |
|---|---|
| Command | Shows the location of the disassembler executable file; default is ${HC08Tools}/decoder. You can specify additional command line options for the disassembler; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the linker will be called with. |
| Expert Settings | |
| Command line pattern | Shows the command line pattern; default is ${COMMAND} ${FLAGS} -O${OUTPUT_PREFIX}${OUTPUT} ${INPUTS} |