Use the Burner for HCS08 Preference Panel to map *.bbl (batch burner language) files to the Burner Plug-In. When the project folder contains a *.bbl file, *.bbl file processing during the post-link phase uses the settings in the Burner preference panel.
The following table lists and describes the burner options for RS08.
| Option | Description |
|---|---|
| Command | Shows the location of the burner executable file. Default value is: "${HC08Tools}/burner". You can specify additional command line options for the burner; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the burner will be called with. |
| Expert Settings | Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${INPUTS}. |
| Command line pattern |