S08 Burner > Output > Configure S-Record

Use this panel to control how the burner generates the output file, as well as error and warning messages. You can specify whether to allocate constant objects in ROM, generate debugging information, and strip file path information.

The following table lists and describes the general options for HCS08 configure S-Record.

Table 1. Tool Settings - Burner > Output > Configure S-Record Options
Option Description
DIsable all (-Ns) Disables generation of all start (S0) and end records (S7, S8, or S9)
No path in S0-record Removes the path (if present) from the file name in the S0 record
No S9-record Disables generation of S9-record
No S8-record Disables generation of S8-record
No S7-record Disables generation of S7-record
No S0-record Disables generation of S0-record