S08 Burner > General

Use this panel to specify the general linker behavior.

The following table lists and describes the general burner options for HCS08.

Table 1. Tool Settings - Burner > General Options
Option Description
Other flags Specify additional command line options for the burner; type in custom flags that are not otherwise available in the UI.