Use this panel to specify the preprocessor settings of the HCS08.
The following table lists and describes the preprocessor options for HCS08.
| Option | Description |
|---|---|
| Command | Shows the location of the preprocessor executable file. You can specify additional command line options for the preprocessor; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the assembler will be called with. |
| Expert Settings | |
| Command line pattern | Shows the command line pattern; default is ${COMMAND} -Lp ${FLAGS} ${INPUTS}. |