ARM Ltd. Windows GCC Linker

Use the ARM Ltd. Windows GCC Linker panel to specify the linker behaviour. The following table lists and describes the various options available on the ARM Ltd. Windows GCC Linker panel.

Table 1. ARM Ltd. Windows GCC Linker
Option Description
Command Shows the location of the assembler executable file.
All options Shows the actual command line the assembler will be called with.
Expert Settings Command line pattern Shows the expert settings command line parameters; default is "${VSPAGCCToolsDir}/${COMMAND}" ${FLAGS} ${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}
Command Shows the location of the assembler executable file.