ARM Ltd. Windows GCC Disassembler

Use this panel to specify the command, options, and expert settings for the GCC disassembler settings. The following table lists and describes the various options available on the GCC Disassembler panel.

Table 1. ARM Ltd. Windows GCC Disassembler
Option Description
Command Shows the location of the GCC compiler executable file used for building the project.
All options Shows the actual command line the compiler will be called with.
Expert settings Shows the expert settings command line parameters; default is "${ARMSourceryDir}/${COMMAND}" ${INPUTS} ${FLAGS}
Command line pattern