Use the ARM Ltd. Windows GCC C Preprocessor settings to specify specify the command, options, and expert settings for the preprocessor.
The following table lists and describes the various options available on the ARM Ltd. Windows GCC C Preprocessor panel.
| Option | Description |
|---|---|
| Handle Directives Only (fdirectives-only) | Check this option to specify the -fdirectives-only command to the preprocessor to handle only directives. |
| Print Header File Names (-H) | Check this option to specify the -H command to the preprocessor if you want to print header filenames. |
| Do not search system directories (-nostdinc) | Check this option if you do not want the assembler to search the system directories. By default, this checkbox is clear. The assembler performs a full search that includes the system directories. |