ARM Ltd. Windows GCC C Preprocessor > Directories

Use the ARM Ltd. Windows GCC C PreprocessorDirectories panel to include paths.

Table 1. ARM Ltd. Windows GCC C Preprocessor > Directories
Option Description
Include User Search Paths (-i) Enables you to add new directories to the list of directories where the user files are searched. Note: Manually edit the absolute paths if the project is moved to a new location. The path will be correct, however, for the location in which the project was originally created. Furthermore, it is a good idea to open the settings of the new project and click 'Apply' to avoid the problem of disappearing user-added include paths.