ARM Ltd. Windows GCC C Preprocessor

Use the ARM Ltd. Windows GCC C Preprocessor to specify specify the command, options, and expert settings for

the preprocessor.

The following table lists and describes the various options available on the ARM Ltd. Windows GCC C Preprocessor panel.

Table 1. Tool Settings - ARM Ltd. Windows GCC C Preprocessor
Option Description
Command This option shows the location of the linker executable file.
All options This option shows the actual command line the linker will be called with.
Expert settings This option shows the expert settings command line parameters; default is "${ARMSourceryDir}/${COMMAND}" ${INPUTS} ${FLAGS}
Command line pattern