Editing Connection

To edit a remote system connection, click the Edit button in the Main tab of the Debug Configurations dialog box.

The Properties for <project_connection> dialog box appears. Here, <project_connection> is the name of the project followed by the associated connection. For example, Proj_01_MC9S08AC128_PnE Full Chip Simulator.

The remote system options in the Properties for <project_connection> dialog box change depending on the selected connection.

Figure 1. Properties for <project_connection> Dialog Box
Properties for <project_connection> Dialog Box

The following table lists the remote system options available in the Properties for <project_connection> dialog box.

Table 1. Properties for <project_connection> Dialog Box
Option Description
Parent profile Specifies the parent profile.
Name Specifies the name of the connection used.
Template Select the remote system template you want to use.
Edit Click to edit the system type. Note: For more information on editing system types, refer to the topic Editing System Types in the chapter Multicore Debugging.
New Click to create a new remote connection.
Connection type Specifies the type of the connection in use. The list is populated based on the selected remote system type and system type. Note: The options in the Connection sub tab will change depending on the selected connection.
Connection Enables you to specify connection settings for the selected connection type. For more information, refer to the topic Connection Tab Settings.
Initialization Enables you to specify initialization settings for the selected connection type. For more information, refer to the topic Initialization Tab Settings.
System Enables you to specify system settings for the selected connection type. For more information, refer to the topic System Tab Settings.
Advanced Enables you to specify advanced settings for the selected connection type. For more information refer to the topic Advanced Tab Settings.
Buttons
  • OK - Click to apply changes and close the Properties for <project_connection> dialog box.
  • Cancel - Click to close the Properties for <project_connection> dialog box without applying the changes.