Target Family : MCF5485
MEMORY { vectorram (RWX) : ORIGIN = 0x20000000, LENGTH = 0x00000400 userram (RWX) : ORIGIN = 0x20000400, LENGTH = 0x00001A00 code (RX) : ORIGIN = 0x10010000, LENGTH = 0x00008000 }
CRC SEED = 0xFEF FILL = 0xFF FROM 0x10010000 TO 0x10010004; //range from code segment DEST = 0x10017FFA
*** PROGRAM SEGMENT 7 *** 0x10010000: 20 00 1F FC 10 //memory range 0x10010000 To 0x10010004
*** PROGRAM HEADER TABLE *** no type offset vaddr paddr filesz memsz flags align 0 LOAD 0x00000154 0x20000000 0x20000000 0x00000000 0x00000000 0x00000007 4 1 LOAD 0x00000154 0x20000400 0x20000400 0x00000000 0x00000000 0x00000007 4 2 LOAD 0x00003674 0x20000400 0x10013520 0x00000018 0x00000018 0x00000007 4 3 LOAD 0x0000368C 0x20000418 0x20000418 0x00000000 0x00000004 0x00000007 4 4 LOAD 0x0000368C 0x2000041C 0x2000041C 0x00000000 0x00000000 0x00000007 4 5 LOAD 0x0000368C 0x2000041C 0x10013538 0x00000018 0x00000018 0x00000007 4 6 LOAD 0x00000154 0x10010000 0x10010000 0x00000000 0x00000000 0x00000005 4 7 LOAD 0x00000154 0x10010000 0x10010000 0x00000400 0x00000400 0x00000005 4 8 LOAD 0x00000554 0x10010400 0x10010400 0x00003120 0x00003120 0x00000005 4
*** PROGRAM SEGMENT 9 *** 0x10017FFA: 16 86 //calculated checksum value -2 bytes
*** PROGRAM HEADER TABLE *** no type offset vaddr paddr filesz memsz flags align 0 LOAD 0x00000174 0x20000000 0x20000000 0x00000000 0x00000000 0x00000007 4 1 LOAD 0x00000174 0x20000400 0x20000400 0x00000000 0x00000000 0x00000007 4 2 LOAD 0x00003694 0x20000400 0x10013520 0x00000018 0x00000018 0x00000007 4 3 LOAD 0x000036AC 0x20000418 0x20000418 0x00000000 0x00000004 0x00000007 4 4 LOAD 0x000036AC 0x2000041C 0x2000041C 0x00000000 0x00000000 0x00000007 4 5 LOAD 0x000036AC 0x2000041C 0x10013538 0x00000018 0x00000018 0x00000007 4 6 LOAD 0x00000174 0x10010000 0x10010000 0x00000000 0x00000000 0x00000005 4 7 LOAD 0x00000174 0x10010000 0x10010000 0x00000400 0x00000400 0x00000005 4 8 LOAD 0x00000574 0x10010400 0x10010400 0x00003120 0x00003120 0x00000005 4 9 LOAD 0x0000F864 0x10017FFA 0x10017FFA 0x00000002 0x00000002 0x00000004 0
New segment added by the post linker or crcgen utility.