S12Z Linker > Link Order

Use this panel to control the order in which the linker receives the object files.

The following table lists and describes the link order options.
Table 1. Tool Settings - Link Order Options
Option Description
Customize linker input order Select if you want the linker to receive the object files in the specified order.
Link Order Lists the object files corresponding to the source files specified in the "link order" list. This option is enables only if Customize linker input order is selected.